Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there load slip monitoring function available in ATV9xx drives for hoisting application.
Yes, load slip monitoring function is available in ATV9xx drives having minimum firmware version v2.1IE17#11 for ATV9xx wall mounting and
ATV9xx floor-standing drives.
There are two ways to manage load slip detection. (1) Generating error ndCF [Load Mvt Error] or (2) bSA [Load Mvt Warn].


In closed-loop mode only. Out of the brake sequence (after [Time to restart] TTR time) and depending [BRH b4] BRH4 setting, triggering of
an error or activation of the speed loop at zero if a movement, for which no command has been given, occurs (measurement of a speed
greater than a fixed minimum threshold determined by [BRH_b4_freq] BFDT).

This parameter can be accessed if [Access Level] LAC is set to [Expert] EPr.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings