Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Customization of CID file of ION7650
For the following parameters, availability of the data objects &  adding the data to an existing dataset,


1.    RMS Voltage
2.    RMS Current
3.    Voltage Flickers
4.    Detection and capture of Voltage Swells and Sags
5.    Detection and capture of Transient Events

For Voltage & Current, they are available in MMXU logical node.
But unfortunately, for others, there is no default logical nodes or data objects available in the ICD templates.
Refer the document for more details & implementation.

In all ION meters, the implementation of IEC61850 is very similar, the measurements available are defined in the modules IEC61850, the only module officially recognized as configurable is the GGIO Cust AI and DI modules.
These modules have the ability to link new registers.
There is a limit of 1 module of each and the number of inputs to the module cannot be changed. The name of the measurement in IEC61850 can also not be changed.

So the conclusion is that you can add the data in the dataset using CET850  & there are no default data objects for your  Voltage Flickers;  Detection and capture of Voltage Swells and Sags & Detection and capture of Transient Events

Schneider Electric India

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings