Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How ISaGRAF Workbench can be connected to an SCADAPack E RTU.
ISaGRAF Workbench can be connected to an SCADAPack E RTU in a number of ways:

- ISaGRAF local serial communications - up to 2 serial port workbench connections are simultaneously supported
- ISaGRAF Ethernet communications - a single TCP/IP workbench connection is supported
- ISaGRAF - DNP3 communications - a single connection via any DNP3 interface is supported (serial, Ethernet, USB)

The above connections are supported in any combination to both RTU ISaGRAF target kernels. Only one active connection is available to a particular target at a time.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings