6 Digit IOA addressingis not possible with Scadapack RTU for IEC 60870-5 address points.
The valid IEC 60870-5-101/104 configuration attributes for an analog point are listed as follows:
The Information Object Address (IOA) parameter is the IEC 60870-5 address for the point. It needs to be a unique value from 1 to 65535. 6553565535.
The Application Service Data Unit (ASDU) parameter is the type of Application Service Data Unit for the point. The valid ASDU types for binary points are:
·1 - Singe-point information
·3 - Double-point information
·45 - Single command
·46 - Double command
·47 - Regulating step command
·58 - Single command, time tag
·59 - Double command, time tag
·60 - Regulating step command, time tag
Released for: Schneider Electric India