System alarms monitor system entities, such as online status for SmartX servers or field devices. The system alarms are generated by the EcoStruxure Building Operation software. Users cannot create new system alarms. The possible causes of a system alarm are gathered in an enumeration called System alarm ID. When a system alarm is triggered, the cause of the alarm is indicated in the System alarm ID column in the Alarms pane or Alarm View. Some system alarms have additional information in the Alarm text column.
Refer below link for the list of all System Alarms:
https://ecostruxure-building-help.se.com/bms/topics/show.castle?id=9801&locale=en-US&productversion=3.0
Refer below link for the list of all System Alarms:
https://ecostruxure-building-help.se.com/bms/topics/show.castle?id=9801&locale=en-US&productversion=3.0
Released for: Schneider Electric India