Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to set On-battery runtime in UPS SRC1KXLI ?
Kindly find the steps to configure battery runtime for UPS SRC1KXLI.
1. Press SELECT button to enter the UPS settings.
2. Navigate through the parameters using SELECT button.
3. Press ENTER/MUTE button to edit -battery runtime. The icon starts flashing to indicate it is ready for editing.
4.Allows the user to set up runtime. When 0 is selected, the runtime will be only 10 seconds.
When 999 is selected, the runtime setting is disabled. The UPS will operate until battery is running out.
5.Press ENTER/MUTE button to Select desired option,the flashing of icon stops after the selection.
6.Select program00 to exit the navigation menu.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings