1.) The ultrasonic frequency of CCT551011 = ? . As per requirement is range 25 kHz to 40 kHz: 32.8 kHz
2.) Radio frequency interference Immunity = ? .As per requirement is 15V/m at 10Hz to 1000MHz. This product has CE certification and was tested against the EMC Directive 2014/30/EU. It’s fulfilling the legal requirements.
3.) The speed of detection for major motion =? As per requirement is 0.5m/s to 1.5m/s: is fulfilled.
4.) it can detect minor motion or fine motion (small movement, the turning of book pages...) yes fulfilled but the same comment as for item 5
5.) The minimum size of thing detection =? Not possible to specify. The faster the movement of the “thing” and the higher the temperature of the surface of the “thing” the smaller it could be….
6.) The operating temperature of this motion sensor? 0°C - +45°C
Released for: Schneider Electric India