Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the classification of the GV2 motor protection switch at altitudes above 2000 m be used.
For use at altitudes between 2000 m and 5000 m above sea level. there are the following classifications for the motor
protection switch of the GV2 series:

2000 m => Umax 690V with Ir

3000 m => Umax 550V with 0.96 x Ir
4000 m => Umax 480V with 0.93 x Ir
5000 m => Umax 420V with 0.90 x Ir.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings