The cold stator resistance or rSC parameter is required for applications that require high performance and to improve the low speed performance of the motor, whatever be the thermal state of the drive or motor.
The value of resistance is in mOhms. It is highly recommended for mechanical handling applications.
Check the attachment for setting of this parameter.
The value of resistance is in mOhms. It is highly recommended for mechanical handling applications.
Check the attachment for setting of this parameter.
Released for: Schneider Electric India