Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does BMENUA0100 supports IPv6 IP addressing.
Yes,BMENUA0100 have Dual IP stack that supports both IPv4 (32 bit) and IPv6 (128 bit) IP addressing:
  • Both IPv4 and IPv6 are configured for the module.
  • IPv6 configuration can be static or dynamic (via SLAAC).
  • IPv4 default setting is auto-assigned based on the module MAC address,if an IP address is not configured.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings