Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Altitude Specifications for XB5*N (Indian range push button )

As per your XB5* rule for equipment compliant with IEC60947-5-1 there is no derating under 2000 meter.

So XB5..N can be used up to 2000 meter

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings