Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to do commands to redundant power supply in m50 and what functions i can carry out.
The PWS_CMD function block is used to control redundant power supplies in a Modicon M580 PAC main rack with an Ethernet backplane (local or remote rack, other connected Modicon M580 PAC).

PWS_CMD function block provides the following command:
1.Swap master and slave power supplies.
2.Clear some diagnostic counters.
3.Start a power supply auto-diagnostic.

The power supply command is built with the PWS_CMD_DDT DDT type.
The additional parameters EN and ENO may also be configured. For more details refer the attachment.

NOTE: Redundant power supplies function is available on CPUs with OS firmware V2.12 or later, and BMECRA31210 communication adapters with firmware V2.16 or later.

Schneider Electric India

Attachment(s)
pws_cmd.pdf [333.63 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings