The table below shows the life of TSXPLP01 battery used in Premium range of processors, even if the power is completely off.
| Ambient Temperature When Inoperative | 30°C | 40°C | 50°C | 60°C |
| PLC off for 12 hours per day | 5 Yrs | 3 Yrs | 2 Yrs | 1 Yr |
| PLC off for 1 hour per day | 5 Yrs | 5 Yrs | 4.5 Yrs | 4 Yrs |
Released for: Schneider Electric India