Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Operating System requirements for Geo SCADA Mobile Server bundled with Geo SCADA 2020.
Refer to the following table for supported Operating System versions:

GeoScada mobile 2020 operating system.JPG

We strongly recommend using a server operating system for Geo SCADA Mobile.
We also recommend for performance and security that a separate server is used for Geo SCADA Server and Geo SCADA Mobile.

The following specifications are also required for the ClearSCADA Mobile Server:
  • Internet Information Server (IIS) 7 (or later) installed with ASP.NET 4.0 (or later)
  • NET Framework 4.5.1 Full or later
  • Minimum 1GHz processor
  • Minimum 2GB RAM, 4GB recommended
  • Minimum 2GB disk space (64-bit version) (includes allowance for .NET framework)
  • Access to Internet or Wireless Virtual Private Network (VPN) for the mobile devices
  • Network access to Geo SCADA Mobile Companion(s)

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings