Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to reset the connection key of Proface HMI ?

The connection key of Proface HMI can be reset by initializing internal memory of the HMI in offline mode.

Below is the procedure to initialize internal memory:

  1. Enter offline mode and touch [Initialization Menu] in the item change over buttons.
  2. [Initialization Menu] screen opens. Touch [Initialize User Memory].
  3. From the [Initialize User Memory] screen, touch the input field and type "1101" (when the [System Password] is [Disable]) or type the defined system password.
  4. Touch [Start].
  5. [Is that really alright] confirmation message appears. Touch [Yes].
  6. When a message appears indicating initialization is complete, touch [Close].

This procedure will reset/delete the old connection key of the HMI.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings