Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can we renew DHCP for BACnet/IP controller in order to renew its DHCP lease with the DHCP server.

You renew DHCP in order to force the BACnet/IP Controller to renew its DHCP lease with the DHCP server.

- In WorkStation, in the System Tree pane, expand the BACnet/IP Controller and then select System .

- In the List View , click IP Network Setting s .

- In the Actions menu, point to IP commands and then click Renew DHCP .

TIP: Renewing DHCP does not become effective until you click Activate changes in the IP commands menu. Activating changes causes the BACnet/IP Controller to apply the changes and then automatically perform a warm start.

Schneider Electric India
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
  • Contact support - +1800-103-0011
  • Price List
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings