오늘 무엇을 도와드릴까요?

What is the part number for the Altistart 48 keypad?

Issue:
Altistart 48 keypad part number request

Product Line:
Altistart 48

Environment:
All serial numbers

Cause:
Customer is looking for the part number of cable used with the remote keypad:  VW3G48101.

Resolution:
The open type ATS48 soft starter keypad is part of the main control board and is not removable from the control board. To replace this integral keypad display, order a control board, VX4G481.
The remotely mounted keypad part number is VW3G48101. This part number includes the keypad, mounting hardware and 3 meter cable.
NOTE:  This does not work with the ATS480.


KEYPAD