오늘 무엇을 도와드릴까요?

Do QED switchboards come with any Lifting Brackets/ Spanner Bars, Straps, Riggings, or Rollers?

Issue:
QED switchboards includes Lifting Brackets / Spanner Bars, Lifting straps, or Rollers

Product Line:
QED SWBD

Environment:
Installation

Cause:
Rigging

Resolution:
Schneider Electric provides lifting straps as standard equipment for NEMA Type 1 switchboard shipping sections rated 3,000 A or less.
Lifting straps are NOT furnished on shipping sections rated more than 3,000 A, or on Outdoor (Nema 3R) switchboards.
Spanner bars , brackets, riggings , or rollers are not furnished  for any SWBD's shipped and are provided by end user.


Detailed information can be found in Instruction Bulletin 80043-055-12, Power-Style QED-2 Switchboards. This bulletin is attached for reference.

슈나이더 일렉트릭 Korea

첨부 파일
80043-055-12.pdf [5.68 MB]