오늘 무엇을 도와드릴까요?

ATV71/ATV61: What is the speed/torque loop response time ?

Goals and Symptoms

What is the speed loop response time within the ATV71?
What is the torque loop response time within the ATV71?

Causes and Fixes

The torque and the speed loop response time is 2mSec +/- 0,5mSec. These value are dependent on the setting of the loop to your application.