Goals and Symptoms
Lexium32M Profibus:
What is the functionality of the "Drive Profile Lexium 2" ?
Causes and Fixes
In the attachet ppt file you can find all informations about the "Drive Profile Lexium 2".
A programm example for Siemens Step7 (S7300/400) is available in the M&D TIP database: (Programming Examples -> Lexium32).
Attachments
(Removed File URL: 202810_F1CE/Drive_Profile_Lexium_2.ppt)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/b90b3bd6b2c6dbcec12577520052a065/fl_block_5/0.62E?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL202810 V1.0, Originally authored by StKu on 06/30/2010, Last Edited by StKu on 06/30/2010
Related ranges: Lexium 32
게시 대상: 슈나이더 일렉트릭 Korea