오늘 무엇을 도와드릴까요?

Why is my 140NOA61110 showing an error E06?

Issue

Why is my 140NOA61110 shwoing an error E06?

Product Line

INTERBUS

Environment

140NOA61110

Resolution

This error indicates that the modules was able to confirm that it's configuration matched the real world network but, it cannot start the buss due to too many transmission errors. This typically indicates wiring problems.