What logic instruction can be used to check the status of my Peer Cop communications?
Issue
What logic instruction can be used to check the status of my Peer Cop communications?
Product Line
Concept
Environment
Concept
Resolution
In 984LL, MSTR function code 9 (Peer Cop Health) or in IEC, MBP_MSTR function code 9 (Peer Cop Health) can be used to check the status of Peer Cop communications for both Specific and Global Peer Cop links. For detailed instruction on the usage of these instructions, please see the help file in your programming software.
게시 대상: 슈나이더 일렉트릭 Korea