Symptoms
The Unity-Pro project is transferred through the USB port and the connection is lost just after the Run command.
The animation remains frozen and the following message is displayed :
"PLC failed - Automatic return to off line"
The PLC remains in Run mode, every time you try to connect it again the same message is displayed.
How to fix
The connection is lost because the project has a long Scan Time and the request takes more time than the driver timeout to get an answer.
You have to change the timeout of the driver, for that :
- Under Unity-Pro, select in the menu PLC -> Set Address,
- In the PLC area, click on the "Communication Parameters" button,
You can increase the Timeout to 10 seconds in order to stay connected.
-Click OK to validate.
게시 대상: 슈나이더 일렉트릭 Korea