What programming software is required to support the TSX07 Nano PLC?
Issue
Need to identify the programming software for the TSX07 Nano PLC.
Product line
PL7-07, TSX Nano
Environment
TLXLPL707P40M
Resolution
PL7-07 is required to support the TSX 07 Nano PLC. The part number for a single install is TLXLPL707P40M. Note that this is an obsolete DOS based software. There is no windows based equivalent software.
게시 대상: 슈나이더 일렉트릭 Korea