오늘 무엇을 도와드릴까요?

Where do I find the USB cable driver for the XBTZG935 cable or for HMISTU/HMISCU?

Issue
Where do I find the USB cable driver for the XBTZG935 cable or for HMISTU/HMISCU?

Product Line
Vijeo Designer
XBTZG935 USB transfer cable

Resolution
This driver is included when you install Vijeo Designer HMI editing software.
It can be also be downloaded here in this FAQ.

The file is attached as "XBTZG935Setup.zip"
Unzip the file and extract "XBTZG935Setup.exe".

슈나이더 일렉트릭 Korea

첨부 파일
XBTZG935Setup.zip [280.32 KB]