What do I do if PLC Label-it software creates a label that does not fit in the module I want?
Both PLC Label-it for Concept and PL7 allow the user to RESIZE each label that is created. You can adjust the Text font size, the width of each label field, the height of each label field, and the spacing above and below each field. The default spacing will work for all Quantum modules. The default spacing for the PL7 version will work for 16 point Premium modules and full height TSX Micro modules. By resizing the labels you can fit 32 point Premium modules and even 16 point half height TSX Micro modules. Momentum module labels can be created and placed sideways in the momentum tophat.
Legacy KB System (APS) Data: RESL1897 V1.0, Originally authored by on , Last Edited by on
Related ranges: Concept
게시 대상: 슈나이더 일렉트릭 Korea