What is the maximum Modbus port speed on the M340 CPU?
Modbus port speed up to 38400 baud on all CPU's with embedded Modbus ports. (ex. BMXP341000, BMXP342000, BMXP342010, BMXP342020)
게시 대상: 슈나이더 일렉트릭 Korea




Modbus port speed up to 38400 baud on all CPU's with embedded Modbus ports. (ex. BMXP341000, BMXP342000, BMXP342010, BMXP342020)