What is the level of protection to the mechanical shocks of the XB5S: IK index.
Goals and Symptoms
What is the level of protection to the mechanical shocks of the XB5S: IK index.
Facts and Changes
XB5S
Mechanical shocks
IK
Causes and Fixes
The XB5S is IK03.
Legacy KB System (APS) Data: RESL200556 V1.0, Originally authored by LaBe on 11/23/2009, Last Edited by LaBe on 11/23/2009
Related ranges: Harmony XB5S