Why is the wireless pushbutton XB5R adapted to industrial application ? What are the free fields operational distances ? How to use the relay ante...
Goals and Symptoms
Why is the wireless pushbutton XB5R adapted to industrial application ?
What are the free fields operational distances ?
How to use the relay antenna ?
Facts and Changes
Harmony wireless
XB5R
Relay antenna
ZBRA1
Robustness
Operational distances
Causes and Fixes
Please, see attachment.
Attachments
(Removed File URL: 206058_1B1A/XB5R_-_Sensing_distances_and_robustness.ppt)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/db73f6eef69fb9d4c12579050052b06d/fl_block_5/0.596?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL206058 V2.0, Originally authored by LaBe on 08/31/2011, Last Edited by CeTa on 09/08/2011
Related ranges: Harmony XB5R
게시 대상: 슈나이더 일렉트릭 Korea