오늘 무엇을 도와드릴까요?

QEIO Ethernet Interlink cables


QEIO Ethernet Interlink cables.
Required for an architecture with combined Ethernet RIO and Ethernet DIO devices.
To be connected between the Ethernet 140NOE771xx communication module and the 140CRP31200 head adaptor.
Cable Length 1 m

Standard version TCSECN3M3M1S4
UL version TCSECN3M3M1S4U