What would cause the message "the module requires a voltage capacity that isn't available from the power supply" error on a Unity Pro build when using a BMXCPS2010 power supply?
The BMXCPS2010 power supply does not have a 24 Vdc output to power any of the 24 Vdc output APS_SENSORS. This is just a warning and can be ignored because you have to use an external supply to power the modules.
게시 대상: 슈나이더 일렉트릭 Korea