Is there a table showing the Icu kA ratings for the LR2K range of overloads?
Goals and Symptoms
Is there a table showing the Icu kA ratings for the LR2K range of overloads?
Range
LR2K
Causes and Fixes
The LR2K is a protection product and we don't fix a value of Icu to these overloads as these do not isolate the circuit as a short circuit protection device.
The Icu value is only relevant to the circuit breakers as they are designed to break circuit current. These have which have some breaking capacity values such as Ics and Icul