브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
Can the designer pop up 'Unintended Equipment Operation' be disabled

Issue
When Designer is launched the following warning message pops up:
Warning => 'Unintended Equipment Operation' pop up

Product Line
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Power Monitoring Expert 2024

Environment
Designer

Resolution
This pop up exists for legal reasons to address product safety and liability, and it cannot be disabled.