오늘 무엇을 도와드릴까요?

PME - Required IEC61000-4-30 report measurement parameters

Issue

There is a need to configure meters for the IEC61000 reports in PME.

Product Line
ION Enterprise 5.x
ION Enterprise 6.x
StruxureWare Power Monitoring 7.x
Power Monitoring Expert 7.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment

Reports


Resolution

Below is the list of measurement names that the 4-30 report requires from a meter:


2-hour report:
===========
'Voltage Flicker Plt on Input V1'
'Voltage Flicker Plt on Input V2'
'Voltage Flicker Plt on Input V3'
'Power Quality Event 2-hour Status'
'Voltage Magnitude 2-hour Mean on Input V1'
'Voltage Magnitude 2-hour Mean on Input V2'
'Voltage Magnitude 2-hour Mean on Input V3'
'Voltage Total Harmonic Distortion 2-hour Mean on Input V1'
'Voltage Total Harmonic Distortion 2-hour Mean on Input V2'
'Voltage Total Harmonic Distortion 2-hour Mean on Input V3'
'Voltage Dip 2-hour Mean as Percentage of Nominal on Input V1'
'Overvoltage 2-hour Mean as Percentage of Nominal on Input V1'
'Voltage Dip 2-hour Mean as Percentage of Nominal on Input V2'
'Overvoltage 2-hour Mean as Percentage of Nominal on Input V2'
'Voltage Dip 2-hour Mean as Percentage of Nominal on Input V3'
'Overvoltage 2-hour Mean as Percentage of Nominal on Input V3'
'Voltage Unbalance Negative Sequence Component 2-hour Mean'
'Voltage Unbalance Zero Sequence Component 2-hour Mean'
'Power Frequency 2-hour Mean'


10-minute report:
===========
'Voltage Flicker Pst on Input V2'
'Voltage Flicker Pst on Input V3'
'Voltage Flicker Pst on Input V1'
'Power Quality Event 10-minute Status'
'Voltage Magnitude 10-minute Mean on Input V1'
'Voltage Magnitude 10-minute Mean on Input V2'
'Voltage Magnitude 10-minute Mean on Input V3'
'Voltage Total Harmonic Distortion 10-minute Mean on Input V1'
'Voltage Total Harmonic Distortion 10-minute Mean on Input V2'
'Voltage Total Harmonic Distortion 10-minute Mean on Input V3'
'Voltage Dip 10-minute Mean as Percentage of Nominal on Input V1'
'Overvoltage 10-minute Mean as Percentage of Nominal on Input V1'
'Voltage Dip 10-minute Mean as Percentage of Nominal on Input V2'
'Overvoltage 10-minute Mean as Percentage of Nominal on Input V2'
'Voltage Dip 10-minute Mean as Percentage of Nominal on Input V3'
'Overvoltage 10-minute Mean as Percentage of Nominal on Input V3'
'Voltage Unbalance Negative Sequence Component 10-minute Mean'
'Voltage Unbalance Zero Sequence Component 10-minute Mean'
'Power Frequency 10-minute Mean'


3-second report:
===========
'Power Quality Event 150/180-cycle Status'
'Voltage Magnitude 150/180-cycle Mean on Input V1'
'Voltage Magnitude 150/180-cycle Mean on Input V2'
'Voltage Magnitude 150/180-cycle Mean on Input V3'
'Voltage Total Harmonic Distortion 150/180-cycle Mean on Input V1'
'Voltage Total Harmonic Distortion 150/180-cycle Mean on Input V2'
'Voltage Total Harmonic Distortion 150/180-cycle Mean on Input V3'
'Voltage Dip 150/180-cycle Mean as Percentage of Nominal on Input V1'
'Overvoltage 150/180-cycle Mean as Percentage of Nominal on Input V1'
'Voltage Dip 150/180-cycle Mean as Percentage of Nominal on Input V2'
'Overvoltage 150/180-cycle Mean as Percentage of Nominal on Input V2'
'Voltage Dip 150/180-cycle Mean as Percentage of Nominal on Input V3'
'Overvoltage 150/180-cycle Mean as Percentage of Nominal on Input V3'
'Voltage Unbalance Negative Sequence Component 150/180-cycle Mean'
'Voltage Unbalance Zero Sequence Component 150/180-cycle Mean'


The ION7650 and ION8800 with the below framework templates or newer will have all the required measurements by default:
7650_FAC-PQ_V3.3.0.0.0
8800A_FAC_V3.3.0.0.0


Even though CM4000s feature IEC61000-4-30 "Anomaly evaluations", it is not supported in the default IEC61000-4-30. The CM4000 stores its IEC61000-4-30 data in a very different way than ION meters do and it would require a new IEC61000-4-30 to be designed.

For the IEC61000-2-4 Report introduced in PME 2022, only the PM8000 and ION9000 are supported. The custom framework located in the following folder will need to be deployed on the meter: ...\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\fmwk\IEC61000-2-4. Note: these custom frameworks replace the entire existing framework. Refer to the PME System Guide for more details.