EGX300 Firmware Version History and Download Information
Issue:
Need to know the latest firmware upgrade available for the EGX300 and the features released with each upgrade.
Product Line:
EGX300
Environment:
EGX300 firmware upgrade
Cause:
The EGX300 periodically receives firmware updates that introduce new features, improvements, and bug fixes. Users may need this information for maintenance, compatibility, or troubleshooting purposes.
Resolution:
See attached file for update history, as January 2026.
Follow link below for EGX300 firmware download:
EGX300 v4.461 Firmware and 4.460 Disk Update | Schneider Electric