Does the embedded Ethernet port on the M340 processors (BMXP342020 or BMXP342030) support IO scanning?
Issue
IO Scanning is needed when using the M340.
Product line
Unity Pro, M340
Resolution
The embedded Ethernet port on the processors (BMXP342020 or BMXP342030) does not support IO scanning.
I/O scanning with the M340 can only be done through a communications module.
Using either a BMXNOE0100, BMXNOE0110 or BMXNOC0401 is required for IO Scanning with all M340 models.