오늘 무엇을 도와드릴까요?

What is the expected operating life of the Circuit Monitor 2000 series LED Display(CM2000)?

Issue
How long will the LED display on a CM2000 series meter operate before failure

Product Line
CM2000 series meter

Environment
Product Longevity

Cause
Operating life of the LED display

Resolution
Due to the high efficiency of the LED's the operating lifetime should exceed 100,000 hours or 11 years of use.