오늘 무엇을 도와드릴까요?

Is sensorless flux vector motor control type available on the ATV61 and ATV71 drives?

Issue:
Is sensorless flux vector available on the ATV61 and ATV71 drives?

Product Line:
Alitvar ATV61 and ATV7

Environment:
All

Cause:
motor control type

Resolution:
Yes, They both have this feature you can access it in Menu 1.4 motor control type and find SVC V.
SVC-V is open loop voltage flux vector control.  It supports operation with a number of motors connected in parallel on the same drive.
This is the default motor control setting on the ATV71 drive and it can be changed to on the ATV61 drives.