브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
Are fuses included with the Powerlogic Energy Meter?

Issue:
The user would like to know if fuses are included with the meter when purchased

Product Line:
Energy Meter

Environment:
Protective Fuses

Resolution:
Fuse Packs/Fuses are not included with the Energy Meter.
The fuses are typically provided by the installer or can be purchased as an accessory called fuse packs.
The fuse packs come with 1/2 A SLO-BLO rating and can be ordered in packs of 1, 2, or 3.

Below are the part numbers for the fuse packs.
EMFP1 Energy Meter Fuse Pack, Set of 1 (includes 1 fuse)
EMFP2 Energy Meter Fuse Pack, Set of 2 (includes 2 fuses)
EMFP3 Energy Meter Fuse Pack, Set of 3 (includes 3 fuses)

Diagram