1. The Red Programme LED flashes after the Programme Button is pressed. This indicates the memory is full. Perform Memory Clearing Procedures to release space.
2. The switch / dimmer does not receive programming commands. Check the position of the function selector at the back of the FreeLocate Switch. Make sure it is in the Programme position.
3. RF wireless control is disabled. (The Programme LED flashes continuously in a pattern of 2). Press the Programme button on the switch / dimmer 6 times within 1 minute. The Programme LED should stop flashing
게시 대상: 슈나이더 일렉트릭 Korea