오늘 무엇을 도와드릴까요?

What are the part numbers of Somachine v4.1?

Issue:
What are the part numbers of SoMachine v4.1?

Product Line:
SoMachine, M238, M241, M251, M258, LMC058

Environment:
PLC Configuration Software

Resolution:
SOMNACCZXSPAZZ    SoMachine V4.1 License Single with DVD disk
SOMNACCZXTPAZZ    SoMachine V4.1 License Team (10) with DVD disk
SOMNACCZXEPAZZ    SoMachine V4.1 License Entity (100) with DVD disk

SoMachine v4.1 is no longer commercialized.
For legacy software licenses, contact:
USA: service.sales@schneider-electric.com
Canada: CDNAutomationServices@schneider-electric.com

Note that the last version of SoMachine was v4.3 (published in 2018).
The current software is called EcoStruxure Machine Expert (2019-present).