Video: How do you set up the ATV61/71 drive so that the set point for PID can be adjusted using the keypad?
Issue:
Trying to set up the ATV61/71 drive so that the set point for PID can be adjusted using the keypad.
Product Line:
ALTIVAR 61, ALTIVAR 71
Environment:
All serial numbers
Resolution:
In the PID Regulator function, set parameter "Act. Internal PID ref" to NO. Use "Ref 1 channel" set to HMI.
“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)“
게시 대상: 슈나이더 일렉트릭 Korea