Is it possible to use Quantum I/O on the M580 ERIO network?
Yes. You will need to have a minimum of Unity Pro XL V11.0 with Hot Fix 1 installed. The Quantum IO will continue to use State RAM addressing.