오늘 무엇을 도와드릴까요?

Can the motor current be permanently displayed on the display of an ATS22 Softstart?

Issue:
Motor current permanently on the display of the ATS22

Product Line:
Altistart 22

Environment:
All Serial number

Cause:
Product feature

Resolution:
Currently, there is no way to select the current to be permanently displayed for the status.
This is possible in our drives and the ATS48, but not in ATS22.