Video: How to display a custom image for an object in a Vista diagram
Issue
A user would like to change the image displayed for a grouping, status, or control object in the Power Monitoring Expert Vista application.
Product Line
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024
Environment
Diagram modifications in the Vista application.
Resolution
See Video below: