Why am I missing data missing after retrieving it using the Vijeo Designer data manager?
1) Make sure to Flush the data. This moves the data from the SRAM to file. The File is either the secondary or optional drive depending on what is selected in the data location. To do that you can execute the FlushAllDataLogging() script command.
2) Periodic data logging in Vijeo Designer only adds a new record when the value change.
2) Periodic data logging in Vijeo Designer only adds a new record when the value change.
게시 대상: 슈나이더 일렉트릭 Korea