브랜드

슈나이더 일렉트릭 코리아 웹사이트에 방문해 주셔서 감사합니다.

슈나이더 일렉트릭 코리아 웹사이트 방문자 분들 모두 환영합니다.
		
오늘 무엇을 도와드릴까요?
How to disable CM4000T Flicker alarms
Issue
The user is unable to disable CM4000T’s Flicker alarms in ION Setup. As shown below, the flicker alarms found in the standard alarm setup are not enabled.
Standard Alarm Setup

Product Line
CM4000T

Environment
ION Setup

Cause
The Power Quality Summary Configuration forces Flicker alarms to stay enabled

Resolution
Navigate to the Power Quality folder after selecting your CM4000T in ION Setup.
The Power Quality Summary Configuration option needs to be disabled in the CM4000T to restrict Flicker alarms.
Power Quality Summary Configuration

After it is disabled, Flicker alarms will be disabled.
PQ Summary