오늘 무엇을 도와드릴까요?

Where can I find information to set up the Bacnet option card on the ATV61 drives?

Issue:
Where can I find information to set up the Bacnet option card (VW3A3319) on the ATV61 drives?

Product Line:
Altivar Machines, Altivar 61, Altivar 71

Environment:
All

Cause:
N/A

Resolution:
For Bacnet setup assistance see the attached Bacnet programming manual.

슈나이더 일렉트릭 Korea

첨부 파일
new card atv61_bacnet_en_NEWCARD.pdf [922.72 KB]