Does Unity Momentum use Base 0 or Base 1 addressing? (Unity is now referred to as Control Expert)
Issue:
Does Unity Momentum use Base 0 or Base 1 addressing? (Unity is now referred to as Control Expert)
Product Line:
Unity Momentum, Control Expert
Resolution:
The Unity Momentum processors use a Base 1 address. The first reference(s) will be %MW1, %IW1, %M1,%I1.
By using the same Base address as the legacy Momentums the process of migrating to Unity is further simplified.
(Unity Pro is now referred to as Control Expert)
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: