오늘 무엇을 도와드릴까요?

Where can I find the operating time (run time) on the ATS48 softstarter?

Issue:
Operating time (run time) on the ATS48 softstarter.

Product Line:
Altistart 48, ATS48

Environment:
All

Cause:
Run time

Resolution:
Go into SUP menu.

RNT parameter is operating time in hours since last reset (if there was ever a reset to begin with).
In hours up to 999 hrs (examples: 001 is 1hr and 111 is 111hrs)
In kilo-hours from 1000-65535 (examples: 1.11 is 1110 hrs and 11.1 is 11100 hrs)
Above 65535 hrs (65.5) the display resets to zero.

Operating time is counted when the motor is not stopped, i.e. when the thyristors fired (heating, acceleration, steady state, deceleration, braking) and in continuous bypass operation.